Technical FAQs

Ask a Question

Can we access M340 or M580 CPU remotely through PMXNOW0300 module.

Yes , it is possible to access M340 or M580 CPU remotely by using Acksys PMXNOW0300 module.

In PMXNOW0300, there are 3 ports available with auto-sensing 10/100 Base TX  and auto MDI-MDIX network interface.
One port is reserved for the M340/M580 CPU or M340/M580 NOE connection.
When connected to the M340/M580 native Ethernet port, PMXNOW0300 ports are considered as “Slave”.
If connected to the M340/M580 NOE Ethernet port instead, PMXNOW0300 ports are considered as “Master”, distributed I/O operation is then fully supported (I/O Scanner).
 
Was this helpful?
What can we do to improve the information ?