Technical FAQs

Ask a Question

Is both the ports of BMXNOR0200H will work parallelly as multiple protocol or at a time only one type of DNP port will work .

Refer the attached document  "NOR_Multiple protocol.JPG", use the appropriate combination of protocol as per the table for multiple protocol on both the ports.
Was this helpful?
What can we do to improve the information ?