Technical FAQs

Ask a Question

Can we use Vijeo Designer v 6.1 runtime license for Vijeo Designer runtime v 6.2.

The license VJDSNRTMPC (Runtime for Magelis iPC) is valid for both versions V6.1 and V6.2. The license is common but not the setup.
Runtime setup file is released  for iPC/PC along with Vijeo designer DVD.
If we earlier has Runtime for 6.1 and want to run 6.2 application, in this case we have to update the Runtime by download (USb cable or Ethernet) or uninstall Runtime V6.1 manually from Add/Remove programs and install Runtime V6.2, the license will be automatically
detected if  Runtime V 6.1 was registered earlier.
Was this helpful?
What can we do to improve the information ?