Technical FAQs

Ask a Question

Is any Function block available in unity pro v 8.0 to deactivate or activate FTP, TFTP, HTTP protocol for M580 Ethernet port.

The EthPort_Control_MX function is used in a Unity Pro V8.0 version, for a Modicon M580 CPU embedded Ethernet, to deactivate or activate the following protocols:
  • FTP
  • TFTP
  • HTTP
Enable the protocol in the configuration before the EthPort_Control_MX function is used to deactivate or re-activate the protocol. 
If a protocol is not enabled in the configuration, the EthPort_Control_MX function does not apply any change and an error is reported.

Refer the attached document  on EthPort_Control_MX for detail.
Was this helpful?
What can we do to improve the information ?