Technical FAQs

Ask a Question

We are not able to connect M580 CPU with unity Loader.

Check if the FTP services are enabled under Cyber Security setting.  If disabled then enable the FTP service in the CPU and download an application to make it work.
Was this helpful?
What can we do to improve the information ?