Technical FAQs

Ask a Question

Which System word can be used to read M580 CPU MAC address, serial number and SD card serial number in unity pro.

The following M580 specific system words that can be used when diagnosing the state of your M580 Hot Standby system: 

%SW132 to %SW134: CPU MAC Address. 
%SW135 to %SW137: CPU serial number 
%SW146 and %SW147: SD card serial number 
Was this helpful?
What can we do to improve the information ?