Technical FAQs

Ask a Question

How to change resolution of output frequency display on embedded display of ATV212 drive.

Resolution of displayed output frequency on embedded display of ATV212 can be changed by changing the parameters F707 and F708 Values.

For example, if both F707 and F708 are equal to 1, the embedded display terminal frequency display will increase only in 1 Hz steps.


 
Was this helpful?
What can we do to improve the information ?