Technical FAQs

Ask a Question

Can We use Analog Output as Digital Output in M171O Controller?


Yes you can use AO1 and AO2 (Analog Output 1 & 2) as open collector digital output.
You need to configure Parameter CL71 & CL72 in Somachine HVAC-Device to 0 to use them as open collector digital output.
 
Was this helpful?
What can we do to improve the information ?