Technical FAQs

Ask a Question

What is difference between Battery back up outlet and surge only outlet ?

1)Back up outlets help provide battery backup power to the connected equipment for a limited period of time during power outages and
voltage fluctuations. The Battery Backup outlets provide battery power to connected equipment only when the Back-UPS is turned on.                                                                                                                                                                                                                                                                                                                                                      2)Surge only outlet helps to provide only surge protection to the connected equipment during voltage fluctuations.
Was this helpful?
What can we do to improve the information ?