Technical FAQs

Ask a Question

How to Recover from a Lost Password in AP5201 ?

Follow the below steps :

1. Turn off the power to the Analog KVM Switch.
2. Open the cover of Analog KVM Switch, and short the jumper marked
"Restore Default Password".
3. With the jumper shorted, turn on power to the Analog KVM Switch, and
wait until the LEDs stop blinking, then turn off the power.
4. Return the jumper to the open position, and replace the cover.
5. Turn the power back on for the Analog KVM Switch. The assigned user
names and passwords will all be cleared. Start the OSD with the
default user name and password.
Was this helpful?
What can we do to improve the information ?