Technical FAQs

Ask a Question

How to activate the OSD main menu in AP5202 ?

Follow the below steps : 

1. If you are already logged in, press the pre-assigned Hot Key (SCROLL
LOCK) twice in rapid succession.2. On initial startup, to access the OSD menus, do either of the following
at the KVM login screen:
ñ Enter a valid username in the username field, press TAB, enter a
valid password in the password field, and press ENTER.
ñ For a first-time KVM activation, or if the username and password
have not been set, leave the username and password fields blank,
and press ENTER.
Optionally, you can assign the control key as the main
menu Hot Key. See OSD HOTKEY.
Æ
USER’S GUIDE
Analog KVM Switch
7
If you logged on as either Administrator or User, the OSD main menu is
displayed. Administrator mode provides access to both Administrator and
User functions and lets you set up operations (including future password authorization). OSD HOTKEY : Selects which Hot Key combination activates the OSD:
press SCROLL LOCK twice or press CTRL twice. The
default Hot Key combination is SCROLL LOCK. The CTRL
Hot Key combination may conflict with other programs
running on computers
Was this helpful?
What can we do to improve the information ?