Technical FAQs

Ask a Question

How to To access any OSD function in AP5202 ?

Follow the below steps : 

To access any OSD function do one of the following:
1. Press the desired function key on your keyboard.
2. Click a function key menu option at the top of the main menu screen.
A submenu provides additional functions related to your selected function
key.
Press ESC, or click the X button in the upper right corner of the OSD, to
return to the previous menu level. 
Was this helpful?
What can we do to improve the information ?