Technical FAQs

Ask a Question

How to activate the SET function in AP5202 ?

Follow the below steps : 

To activate the SET function, press F3 or click the F3 menu option at the top
of the main menu screen.
SET allows an Administrator or User to set up a unique working
environment profile. The stored profile activates each time a corresponding
user logs into the system.
To activate a submenu option, move the highlight bar to the option, and
press ENTER, or double-click the SET function item. An icon to the left of the
menu option indicates your selection.
Was this helpful?
What can we do to improve the information ?