Technical FAQs

Ask a Question

How to SET QUICK VIEW PORTS in ADM submenu function for AP5201 model ?

Follow the below steps :

Quick View ports allow users to scan and view selected
ports, saving time for a large installation base.
Select or deselect a port by moving the highlight bar to the
port and pressing SPACEBAR. An arrowhead in the QV
column on the main menu list indicates ports selected as
Quick View.
Setting a port as a Quick View port causes the following:
ï If a user selects either the QUICK VIEW or QUICK VIEW +
POWER ON options, only those ports selected as Quick
View appear in the main menu list. 
ï If a user selects either the QVIEW or QVIEW + POWER
ON options, only those ports selected as Quick Views are
auto-scanned or accessed through the Skip feature. 
Was this helpful?
What can we do to improve the information ?