Technical FAQs

Ask a Question

How many Link150 can we connect in Ethernet daisy chain and maximum allowed distance between them ?



We have tested up to 32 Link150 devices in Ethernet daisy chain connection.
We are supporting 10/100 Base TX (802.3af) port standard for Link150 so maximum length is 100 meters.
Was this helpful?
What can we do to improve the information ?