Technical FAQs

Ask a Question

What are communication capabilities of Accusine PCS

Communication capabilities are provided below

1.CAN+ Bus communication required for PARALLEL and MASTER /SLAVE configurations
2.MODBUS (Serial and TCP/IP) ports available for EMS & SCADA applications
3.Assignable Digital I/O’s for local indications and control
 
Was this helpful?
What can we do to improve the information ?