Technical FAQs

Ask a Question

How much is IP degree of various terminals of PM5560 ?

1) How much is IP degree of below terminals, without using sealing kit?
- control power (L1,L2)
- voltage inputs (V1,V2,V3,VN)
- status inputs (S1,S2,S3)
- digital outputs (D1+,D1-)
- RS-485
- current inputs  (I1+,I1-,I2+,I2-,I3+,I3-,I4+,I4-)

Answer: IP 10 without sealing kit 

2) How much is IP degree of below treminals, when using sealing kit?

- voltage inputs (V1,V2,V3,VN)
- current inputs  (I1+,I1-,I2+,I2-,I3+,I3-,I4+,I4-)

Answer: IP 20 with sealing kit 

Also, the main purpose of using sealing kit is Tamper proofing.
Was this helpful?
What can we do to improve the information ?