Technical FAQs

Ask a Question

Is it possible to use an additional braking unit together with an AFE.

It is possible to use an additional braking unit together with an AFE(Active Front End). It is only possible for 400V and 440V for ATV71 N4 range and 500V and 600V for ATV71 Y range. At 480V and 690V, it is not possible to combine an AFE and a BU.
Was this helpful?
What can we do to improve the information ?