Technical FAQs

Ask a Question

Is XCMD3902T1 limit switch dedicated for railways applications.

Refer to attached the data sheet of the XCMD3902T1 adapted limit switch dedicated for railways applications because it is supplied with a special cable halogen free certified in compliance
to the railways standards and especially the EN 45545 standard.
.
Was this helpful?
What can we do to improve the information ?