Technical FAQs

Ask a Question

What is the degree of protection (IP) of Canalis KDP busbar trunking.

The degree of protection (IP) of Canalis KDP busbar trunking is IP55.
Was this helpful?
What can we do to improve the information ?