Technical FAQs

Ask a Question

Could you advise the diameter of the jacket for 3 x 0.34 mm² PVR cable for part number XSAV11373 & XSAV12373.

Both part number XSAV11373 & XSAV12373 have 3 wires and use the same cable. Outer jacket has an external diameter of 4.2 mm (data given for information only). 
Was this helpful?
What can we do to improve the information ?