Technical FAQs

Ask a Question

Is it possible to enable and disable the ATV630 PID by DI3 input.


Yes, it is possible to enable and disable the ATV630 PID by DI3 input.
Refer to attached File.
You can assign logic input (example DI3) to PAU (Auto/Manual select input).
when the DI3 is on, the PID will work.
And when the DI3 is off. The PID will not work. 
Was this helpful?
What can we do to improve the information ?