Technical FAQs

Ask a Question

How many I/O cards can be added to the PM2x30.

Any one IO module can be used at a time with PM2130 or PM2230 meter. The control power range with IO module will be 90 t0 300V AC L-N or DC.

Was this helpful?
What can we do to improve the information ?