Technical FAQs

Ask a Question

Please provide the complete list of the error codes in PM2000 meter.

The complete error codes are shown below:

            0 = OK, 1 = Error Detected
            Bit 01 = Summary   (on if any other bit is on - Maintenance Icon shown on HMI )
            Bit 02 = RAM Failure
            Bit 03 = NVRAM Failure
            Bit 04 = RTC Failure
            Bit 05 = Calibration Failure
            Bit 06 = Clipping Detected
            Bit 07 = Over-Running Energy Pulse Output
            Bit 08 = Inp Mtr Diag Rate Exceeded/Backup RAM failure                          
            Bit 09 = Lang File Mis Match
            Bit 10 = Lang String Mis Match         
            Bit 11-16 Not Used
 
Was this helpful?
What can we do to improve the information ?