Technical FAQs

Ask a Question

What is the Ride-through time of AC control power for EM6400NG.

Please find the details below:

80 ms typical at 120 V AC and maximum burden.
100 ms typical at 230 V AC and maximum burden.
100 ms typical at 277 V AC and maximum burden.
Was this helpful?
What can we do to improve the information ?