Technical FAQs

Ask a Question

What are the I/O modules supported by PM2230/PM2130 energy meters ?

                Model                                       Commercial reference                                              Description
2 Channel Digital Input Output Module       METSEPM2KDGTLIO22                 Digital I/O module with 2 channel input and output.

2 Channel Analog Input Output Module      METSEPM2KANLGIO22                 Analog I/O module with 2 channel input and output.

1 Channel Analog Input Output Module      METSEPM2KANLGIO11                 Analog I/O module with single channel input and output.
 
Was this helpful?
What can we do to improve the information ?