Technical FAQs

Ask a Question

What are the characteristics of pulse output of PM2230 energy meter ?

Characteristics of Pulse output (POP) :

Max 40 V DC, 20 mA
20 ms ON time
Configurable pulse weight from 1 to 9999000 (pulse/ k_h)
Was this helpful?
What can we do to improve the information ?