Technical FAQs

Ask a Question

Is SCADAPACK 334 RTU can use 5607 I/O Module for Extension of I/O's. If Compatible how many 5607 Module can be used for one 334 RTU.

Yes, 5607 I/O Expansion module is compatible with Scadapack 334 RTU. A maximum of eight (8) 5607 modules (and 5606 modules together) can be addressed on a 5000 Series
I/O bus.
Was this helpful?
What can we do to improve the information ?