Technical FAQs

Ask a Question

Is it possible to connect ATV660 and ATV680 together with an Active Harmonic Filter on the same mains supply.

Yes, it is possible to connect ATV660 and ATV680 together with an Active Harmonic Filter on the same mains supply.
 
 The combination of ATV660 / ATV680 and Accusine had been tested in the factory. There had been no negative influence to each other.
 
Was this helpful?
What can we do to improve the information ?