Technical FAQs

Ask a Question

What is the measurement in Y 100 parameter on ATV212 drive,If the incoming voltage is 415V.

Y 100 [Line voltage] will be around 415V if parameter F701 is 1.
The average of the 3 phases of line to line input voltages displayed either in volts or as a percentage of the drive's rated input voltage (200 V for 208/240 V models - 400 V for 480 V models). Select % or volts with parameter [Unit value selection] (F701).
Was this helpful?
What can we do to improve the information ?