Technical FAQs

Ask a Question

Does EMC clamp come as standard with ATV312 drive.

 
EMC plate comes as standard with ATV312 drive. EMC clamp does not come as standard with ATV312 drive.
Note: we can order just two diameter clamps Ø 4.8 mm and Ø 7.9 mm cable (reference TM200RSRCEMC). Refer to attached document.
If you want another diameter, then you have to order directly with the local supplier.
 
Was this helpful?
What can we do to improve the information ?