Technical FAQs

Ask a Question

What is the UL file number for XPSAF5130.

UL file number for XPSAF5130 is E164353.
 
Refer to below Link (see pdf page6).
 
http://database.ul.com/cgi-bin/XYV/template/LISEXT/1FRAME/showpage.html?name=NKCR.E164353&ccnshorttitle=Auxiliary+Devices&objid=1074106764&cfgid=1073741824&version=versionless&parent_id=1073990247&sequence=1
 
=>” Safety relays Model(s) XPS-AF, -AFL, -AK, -AV, -MP, -AC, -AR, -ATE, -TSA, -TSW, -DMB, -DME, -BF, -VC, -VNE or -CM, followed by four thru six numbers, may be followed by P, may be followed by T, with or without three numbers”
=>four thru six means it could be 4,5 or 6 digit depending on the module type.
=> may be followed by P, may be followed by T, with or without three numbers.
Was this helpful?
What can we do to improve the information ?