Technical FAQs

Ask a Question

Is it possible to use ATS48 Soft Starter without bypass contactor.

The ATS48 can work without by-pass contactor, but pay attention to not bypass is the drop voltage across the thyristors witch generate power losses and heating. We can say than in 95% of the case the bypass mode is used to prevent this problem principally.
The bypass is use for eliminate the heating inside the ATS48.
 
Was this helpful?
What can we do to improve the information ?