Technical FAQs

Ask a Question

Is ATV61HC50N4 drive 6 pulse.

All drives below ATV61HC50N4 drives are 6 pulse. All drives from ATV61HC50N4 and above are equipped with two rectifier bridges as standard.
These drives can be connected to a 12 pulse mains supply without option.
 
Was this helpful?
What can we do to improve the information ?