Technical FAQs

Ask a Question

How to determine the version of ClearScada Server License.

To determine the version of ClearScada Server software license:

- From the windows system tray on the ClearScada Server  machine , right click on the ClearScada Server Icon  and select 'License Details'.
- If prompted, enter your ClearScada Administrator Username and Password details.
- The License details dialog will be displayed as in attachment.
- Locate the section  of the dialog that dispalys the support version (for example: "up to 6.75 ") identifying the version of ClearScada compatible with your current License.
- Reference this version against your ClearScada version to determine whether you require an update of  your license prior to upgrading.
Was this helpful?
What can we do to improve the information ?