Technical FAQs

Ask a Question

What is the Maximum wire dimension of Vamp 210 relay.

The Maximum Solid or stranded wire dimension of Vamp 210 relay 4 mm2 (10 – 12 AWG).
Was this helpful?
What can we do to improve the information ?