Technical FAQs

Ask a Question

What is the rated frequency of Vamp 57 relay.

The Rated frequency fN is 45 – 65 Hz (protection operates accurately).
Measuring range is 16 – 95 Hz.
< 44Hz / > 66Hz (other protection is not steady except frequency protection).
Was this helpful?
What can we do to improve the information ?