Technical FAQs

Ask a Question

What is M172P controller retentive variable limitation?

The Memory of M172P can be summarized as follows:



Use EEPROM variable for retain data after power recycle. 

Note: The EEprom of TM17* is always read only from IEC Code because it can be written a limited number of times (100K).

 
Was this helpful?
What can we do to improve the information ?