Technical FAQs

Ask a Question

How much is the onboard memory of PM2230 energy meter ?

The onboard data logging memory for PM2x30 is NVRAM . The size of non-volatile memory is 256kB. Up to two fixed parameters (e.g., kWh and kVAh) with configurable interval and duration (e.g., 2 parameters for 60 days at 15 minutes interval) Maximum 5760 records.
Was this helpful?
What can we do to improve the information ?