Technical FAQs

Ask a Question

What is the pollution degree of Compact NSXm circuit breaker.

The Compact NSXm circuit breakers are certified for operation in pollution-degree 3 environments as defined by IEC standards 60947-1 and 60664-1 (industrial environments).
Was this helpful?
What can we do to improve the information ?