Technical FAQs

Ask a Question

Is BMX DDO6402K ,BMX DDO3202K and BMX DDO1602 modules are protected against Short-circuit.

Yes, these modules are having built-in protection against short-circuits and overloads by current limiter and electric circuit-breaker 1.5 In < Id < 2 In.

Refer the attached specification document for reference.
Was this helpful?
What can we do to improve the information ?