Technical FAQs

Ask a Question

Are Compact NSXm circuit breakers compliant for installation in class II switchboards.

All Compact NSXm devices are class II front face devices. They may be installed through the door of class II switchboards (as per IEC standards 61140 and 60664-1)
without downgrading switchboard insulation. Installation requires no special operations, even when the circuit breaker is equipped with a rotary handle.
Was this helpful?
What can we do to improve the information ?