Technical FAQs

Ask a Question

We are getting message "PLC is Still in NOCONF, the downloaded application isn't a valid application" during program download to M580 CPU through Service port.

This message usually come due to installation of CPU on wrong slot or CPU rack address is not set to 0 in case of rack expander module installed on the rack.
Was this helpful?
What can we do to improve the information ?