Technical FAQs

Ask a Question

Is Compact NSXm suitable for isolation with positive contact indication.

All Compact NSXm devices are suitable for isolation as defined in IEC standard 60947-2:
-> The isolation position corresponds to the O (OFF) position.
-> The operating handle cannot indicate the OFF position unless the contacts are effectively open.
-> Padlocks may not be installed unless the contacts are open.
Installation of a rotary handle does not alter the reliability of the position-indication system.

The isolation function is certified by tests guaranteeing:
-> The mechanical reliability of the position-indication system
-> The absence of leakage currents
-> Overvoltage withstand capacity between upstream and downstream connections.
The tripped position does not insure isolation with positive contact indication. Only the OFF position guarantees isolation.
Was this helpful?
What can we do to improve the information ?