Technical FAQs

Ask a Question

What is the degree of protection of Compact NSXm circuit breakers.

The following indications are in accordance with standards IEC 60529 (IP degree of protection) and IEC 62262 (IK protection against external mechanical impacts).

Bare circuit breaker with terminal shields
-> With toggle: IP40, IK07.
-> With direct rotary handle: IP40 IK07.

Circuit breaker installed in a switchboard
-> With toggle: IP40, IK07.
-> With direct rotary handle: IP40, IK07.
-> With extended rotary handle: IP54 or IP65 IK08
Was this helpful?
What can we do to improve the information ?