Technical FAQs

Ask a Question

How can Multi-Monitors be set and what is the maximum number in Vijeo Citect.

For setting MultiMonitors in Citect, following INI patameter need to be set:
[MultiMonitors]
Monitors=1 (Allowable value is upto 8)
For setting up the startup page in each monitor, set the below parameter
[MultiMonitors]StartupPage1 (for monitor 1)
[MultiMonitors]StartupPage2 (for monitor 2)
and so on upto 8.
You will need to include 'CSV_Include' project in your project as this contains the cicode functions for establishing MultiMonitors or you may copy the cicode function in your current project.
Was this helpful?
What can we do to improve the information ?