Technical FAQs

Ask a Question

Which wireless devices can be configured as an End Device in NetBotz Rack Monitor 450 (NBRK0450) ?

Solution : The wireless devices can be configured as an End Device in NetBotz Rack Monitor 450 (NBRK0450) are NBWS100T and NBWS100H.
Was this helpful?
What can we do to improve the information ?