Technical FAQs

Ask a Question

Is line and load reversibility available in Compact NSXm circuit breakers.

The Compact NSXm circuit breakers can be supplied from either the top or the bottom without any reduction in performance.
This capability facilitates connection when installed in a switchboard.
All connection and insulation accessories can be used on circuit breakers supplied either from the top or bottom.
Was this helpful?
What can we do to improve the information ?