Technical FAQs

Ask a Question

After upgrading to SCADA 7.30 or later, alarms will not be displayed after logging in with a user.

This can be due to reason if a User Name having numeric characters (e.g. 12345). With the change of the alarm server backend in SCADA 7.30, users that have
only numeric characters in their username are no longer supported.
Was this helpful?
What can we do to improve the information ?