Technical FAQs

Ask a Question

'Symbol search failed' compilation error after installing the latest patch of Vijeo Citect 2015 Service Pack 1.

The full message is 

Table: C:\Program Files (x86)\Schneider Electric\CitectSCADA 7.50\Bin\SACCUMS.DBF

Error: Symbol search failed

Context: table C:\Program Files (x86)\Schneider Electric\CitectSCADA 7.50\Bin\SACCUMS.DBF symbol ALARMTAGITEM
The reason for this message is that the patch file for the wrong product was installed. A patch for CitectSCADA was installed when the installed product is Vijeo Citect.
Or a patch for Vijeo Citect was installed when the installed product is Citect SCADA. To fix it just uninstall the patch and re-install the correct one.

Was this helpful?
What can we do to improve the information ?